• placeholder
  • All Files

Device Control

Start/stop the Device

With the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger

You can start / stop the device with the buttons and

With the KAS RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running

In the KAS Runtime menu you can click the start / stop command.

Start Device with the Run Time" />

Figure 5-59: Start Device with the KAS Runtime

Log Window

The Log window displays all run-timeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running messages issued by the device or by the KAS Simulator when testing the application.

The log area of the KAS IDE and the KAS Runtime Simulator are the same. It contains the log messages as described in Information and Logs

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen